{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
You are currently viewing the content available in Vietnam. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

Why does the BMENOC03x1 use the XBUS communications?

Issue
BMENOC03x1 use the XBUS  communications

Product Line
M580, BMENOC03x1

Environment
EcoStruxure Control Expert

Resolution

The BMENOC03x1 module uses X Bus communications on the Ethernet backplane to obtain and exchange the below type of data with the M580 CPU:
1.  Configuration data for the BMENOC03•1 module
2.  Application and diagnostic data

Did this answer your question?

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.