Search FAQs
{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
You are currently viewing the content available in Vietnam. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the clock accuracy on the Magelis HMIGTO6310?
The HMIGTO6310 clock can deviate +/- 65 seconds/months but can be as high as -380s / + 90s / months depending on the age of the terminal and temperature.
Attachment(s)
Did this answer your question?