How do you set up a end of damper for the legacy ATV212 S-Flex enclosed drive?

Issue:
End of damper control for a S-flex ATV212 with bypass option.

Product Line:
Altivar

Environment:
Altivar Machine

Cause:
Set up Damper control

Resolution:
End customers auto start will need to start up Damper Solenoid.   Once the Damper is open you will need a damper relay to close (R) to indicate damper is in correct position.
You will need qty 3 end of damper dry contacts.
wire you 3 end of damper dry contacts to:
P24 to R
Terminals 2 to 4
add dry contact in series with R input on the drive.
see the attachment for example diagram.

Schneider Electric Việt Nam

Phần đính kèm

Damper control add.pdfDamper control add.pdf [126.92 KB]
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: