How do you set Preset Speeds on ATV61 or ATV71 drive?
Issue:
Preset Speeds on ATV61/ATV71 drives

Product Line:
ATV61 or ATV71

Environment:
All models, all serial numbers

Cause:
Application requires Preset Speeds

Resolution:
  • Go into 1- Drive menu and then to 1.7 Application function menu.
  • Under 1.7, go into Preset speeds submenu.
  • Set 2,4,8, or 16 Preset speeds to logic inputs as desired.
Speeds for each combination of logic inputs are available at the combination table for preset speed inputs in the ATV61 programming manual.
Refer to ATV61_programming_manual_EN_1760649_08

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: