Does the Multi-Circuit Meter (MCM) device type use 1 device license or multiple device licenses for each circuit in ION Enterprise v5.6 Service Pack 2 (SP2)?

The MCM uses 1 device license for each circuit that it is monitoring. If the MCM is monitoring 8 circuits, ION Enterprise will require 8 device licenses.

Date Created: February 25, 2009
Last Revised: April 29, 2009
Public
Original Author: MN
All content © 1992-2009 Schneider Electric


Legacy KB System (APS) Data: RESL198404 V1.0, Originally authored by MiNe on 04/30/2009, Last Edited by MiNe on 04/30/2009
Related ranges: MCM (Multi-Circuit Meter), ION Enterprise V5.6

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: