Migrating a SPM 7.0.1 system to a new server
Issue
Migrating a SPM 7.0.1 system to a new server.

Product Line
StruxureWare Power Monitoring 7.0.x

Environment
Standalone System

Cause
The system needs to be fully moved to a new server keeping all the configuration, set up and data intact

Resolution
*Warning: This article contains information about editing the registry. Improper changes to the registry can permanently damage the operating system. Always backup the registry before making any changes.*
*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).

*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.*

See the attached document for instructions on how to Migrate a SPM 7.0.1 system to a new server.

Schneider Electric Việt Nam

Phần đính kèm
server_migration.zip [66.96 KB]