Can the mains overvoltage fault be inactivated on the ATV61 and ATV71 drives?
Issue:
Mains overvoltage fault disabling on ATV61 and ATV71 Drives

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Needs to disable the mains overvoltage fault protection on the ATV61 and ATV71 drives.

Resolution:
It is not possible to inactivate the Mains Overvoltage detection in the drive. The trip level threshold and delay are fixed and cannot be changed.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: