What type of material is used for Flite construction?
Flite is constructed using high grade Industrial components as detailed below
  1. Enclosure (part in grey color) : PEHD or High Density Polyethylene is used in the manufacturing of the Flite Enclosure
  2. Transparent  glass part : LEXAN
  3. Attachement Claws : Polyamide for the clip and an Elastomer for the brake block.

Schneider Electric Việt Nam