StruxureWare DCE virtual machine may hang, logs show E1000 NIC error
Issue:
StruxureWare DCE virtual machine may hang, messages log show E1000 NIC error

Product Line:
StruxureWare Data Center Expert

Environment:
StruxureWare DCE virtual machine potentially any version.

Cause:
Potential incompatibility with older Virtual Machine NIC driver.

Resolution:
Looking at DCE log files on a VM install, you may see an error similar to the following: kernel:

e1000 0000:02:00.0: eth0: Detected Tx Unit Hang

This has been seen in VMware ESXi 5.0. It appears to be most prevalent when attempting a DCE backup. In cases where this issue does exist, an upgrade of the VM host to ESXi 5.5 has been seen to resolve this error.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: