Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Why is the Vijeo Designer XBTZG935 USB cable driver not working on Windows 11?

Issue

When trying to download to a HMI via USB cable using Vijeo Designer software on a Windows 11 PC I get the following error message:

XBTZG935 error message

Product Line

Vijeo Designer

XBTZG935 driver

Environment

Windows 11

Cause

Windows 11 introduced new features that are not compatible with the XBTZG935 USB cable driver. One of them being the Hypervisor-Protected Code Integrity. If the system has HVCI enabled and the driver is not compatible with that feature, Error code 39 will be reported by Device Manager to indicate that the driver could not loaded.

Resolution

Disable Hypervisor-Protected Code Integrity using regedit. Here are the steps to do so:

1. Run regedit as admin

2. Locate \HKEY_LOCAL_MACHINE\SYSTEM\ControlSet001\Control\DeviceGuard\Scenarios

3. Check if “HypervisorEnforecedCodeIntegrity->Enabled” is set to 1

4. Modify the register key “Enabled” to 0

5. Restart the computer and test

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)