{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the difference between LX1 and LX9 coil?
Issue:
LX1 and LX9 characteristic

Product Line:
Tesys F line Contactors and Accessories

Environment:
TeSys™ F AC Coils

Resolution:
The LX1 is the standard control type coil. The LX9 low sealed consumption coil offers high tolerance to inrush voltage drops, immune to micro-breaks (main supply or contact chain) and are capable of operation on networks with harmonic numbers less than or equal to 7.

Schneider Electric Global