What external voltage must be supplied for the control on an ATS48?
Published date:
02 April 2019
Issue:
What external voltage can be used for the control on an ATS48?
Product Line:
ATS48 series soft starters.
Environment:
All models, All serial numbers.
Cause:
Clarification of product characteristics needed.
Resolution:
The control voltage for the ATS48 series soft starters has a range of 110V -15% to 230V 50 or 60 Hz. and should be connected to CL1, CL2 terminals.
This voltage powers the display and the electronics in the softstart and is used to generate the 24VDC power supply used for the low voltage controls.
Consult the User Manual for more details.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.