Browse FAQs

What is the part number for the computer cable that will allow connection to a Soft Starter using SoMove or the obsolete PowerSuite software?

Published date: 12 February 2019

Issue:
What is the part number for the computer cable that will allow connection to a Soft Starter using SoMove or the obsolete PowerSuite software?

Product Line:
ATS48
ATS22

Environment:
All part numbers, all models

Cause:
Cable is required for the connection.

Resolution:
TCSMCNAM3M002P is a USB to RJ45 cable that includes the RS485 converter required to communicate to the softstart (and our current VFD products).

NOTE: The old cable kit part number VW3A8106 will also work but requires a DB9 serial port on the PC (or a USB to DB9 adapter)

The SoMove software is available for download from our website:  https://www.se.com/us/en/product-range/2714-somove/?parent-subcategory-id=54405
Also required is the DTM Library for the product.

NOTE:  Powersuite has been obsolete for many years.  It is no longer supported and is not receiving updates.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.