Issue :
Which Relay contact would you land wires on to get a motor running indication from an Altistart 48?
Product Line :
Altistart 48
Environment :
All
Resolution :
To obtain a contact closure indicating motor is running, could set up relay R3 for rnl which changes state when the motor is powered.
This programming is done in the I/O menu of the parameters.
Which Relay contact would you land wires on to get a motor running indication from an Altistart 48?
Product Line :
Altistart 48
Environment :
All
Resolution :
To obtain a contact closure indicating motor is running, could set up relay R3 for rnl which changes state when the motor is powered.
This programming is done in the I/O menu of the parameters.
Released for:Schneider Electric Global