What are the dimensions and the weight on the ATS48C41Y soft starter?
Published date:
12 April 2019
Issue:
What are the dimensions and the weight on the ATS48C41Y, ATSC59Y and ATS48C66Y soft starter?
Product Line:
Altistart 48
Environment:
ATS48C41Y ATSC59Y ATS48C66Y
Cause:
Sizing for application
Resolution:
The entire width of the unit is a = 15.75 in (400 mm), the entire height of unit is b = 26.38 in (670 mm), the entire depth of the unit is c = 11.81 in (300 mm), and the weight is 113.3 lb (51.4 kg).
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.