{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is the memory for the altivar drive settings and parameters, in the drive, or in the keypad?
Issue:
Settings and parameters saved in the drive or keypad.

Product Line:
Altivar 58

Environment:
All

Cause:
N/A

Resolution:
The actual program that the drive uses to run is stored in the drive control board itself. Removal of the keypad will not alter that program.
NOTE: There is storage memory available in the keypad that can be used to save a copy of the parameter settings. This may not be the same as the actual program that the drive is using.

Schneider Electric Global