Issue:
Coating on ATS48 control module.
Product Line:
Altistart 48
Environment:
All
Cause:
Altistart 48 Control Module
Resolution:
There is some degree of conformal coating. The specification on the unit for Maximum ambient pollution is that it conforms to IEC 60664-1, Pollution Degree 3.
Coating on ATS48 control module.
Product Line:
Altistart 48
Environment:
All
Cause:
Altistart 48 Control Module
Resolution:
There is some degree of conformal coating. The specification on the unit for Maximum ambient pollution is that it conforms to IEC 60664-1, Pollution Degree 3.
Released for:Schneider Electric Global