{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What can cause an StF fault on the ATS48 Soft Starter?
Issue:
Remedy for the StF fault

Product Line:
ATS48

Environment:
StF faults

Cause:
n/a

Resolution:
The StF is a fault indicating Excessive starting time. As of December 2004, this fault is not documented in the United States Literature for the ATS48.
To remedy the fault perform the following:
* Check the mechanism (wear, mechanical play, lubrication, blockages, etc.).
* Check the value of tLs setting in the PrO menu.
* Check the sizing of the starter-motor in relation to the mechanical requirement.

Schneider Electric Global