Browse FAQs

Do we offer a option to supply 120 volts for the logic inputs on the ATV61 and ATV71?

Published date: 08 July 2020

Issue:
Using 120V to supply Logic Inputs on the ATV61/71

Product Line:
Atlviar ATV61 and ATV71

Environment:
All

Cause:
Needs to have an option to supply 120 vac to turn on the logic inputs to start up the drive.

Resolution:
Yes,  The 115 VAC logic input adaptor is part number VW3A3101.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.