Can the analog output of the ATV61 or ATV71 be set up as 0-10 VDC instead of 4-20 mA?
Published date:
12 June 2019
Issue:
Can the analog output of the ATV61 or ATV71 be set up as 0-10 VDC instead of 4-20 mA?
Product Line:
ATV61 and ATV71
Environment:
All
Cause:
NA
Resolution:
Yes.
Go to the Input/Output menu (1.5) and set AO1 type to voltage (0-10v range). Set AO1 assignment to the proper setting. The minimum and maxim range can also be adjusted inside the 0-10 V or 4-20 mA ranges.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.