{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What does the 5 indicate before the coil voltage code on the LC1K****5** or LP1K****5** contactors?
Issue:
Does the number 5 on Tesys K contactors refer to the type of termination?

Product Line:
Contactors and Starters-IEC

Environment:
Tesys K Miniature IEC Contactors and Overload Relays

Resolution:
The suffix 5 indicates solder pin terminal connections instead of the standard screw clamp.

Schneider Electric Global