What is the part number for ATV61 and ATV71 Ethernet IP card?
Published date:
07 August 2019
Issue:
What is the part number for ATV61 and ATV71 Ethernet IP card?
Product Line:
Altivar 61 and Altivar 71 drives, all serial numbers
Environment:
All
Cause:
Need part number for Ethernet IP card
Resolution:
The part number for the Ethernet IP card is VW3A3316. This card has Ethernet IP functionality only.
The VW3A3320 option card has Ethernet IP and Modbus TCP functionality.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.