{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Symmetra LX and the InfrastruXure (ISX) Manager Load Reports

Issue

Symmetra LX and the InfrastruXure (ISX) Manager Load Reports - what to expect


Product Line
  • InfrastruXure (ISX) Manager - AP92200
  • Symmetra LX UPS Models

Environment
  • Using ISX Manager reporting
  • All ISX Manager versions

Cause


The Symmetra LX is a split-phase UPS which reports an individual value for load percentage on each of the two "hot" legs that are present.


Resolution


Since the output of multiple phases is being monitored and recorded, the Symmetra LX will appear in the "3-Phase UPS Load" report in ISX Manager and not on the "1-Phase Load" report as is the case with other Symmetras. The third phase in this report will be reported as "Unknown."

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.