ISX Central | Enabling or disabling the private LAN will cause a new self signed SSL certificate to be generated.
Published date:
07 September 2018
Issue:
Enabling or disabling ISX Central Private LAN will cause the server to generate a new self signed SSL certificate
Product Line:
InfraStruxure Central (ISXC)
Environment:
InfraStruxure Central (Prior to 6.2)
Cause:
When working with SSL certs, you will need to re-add the cert if you enable or disable DHCP on the private LAN or if you change IP information on the private LAN. This is a known issue.
Resolution:
This issue was resolved in InfraStruxure Central 6.2
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.