{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Why is the Protection Working LED of an APC SurgeArrest, or SurgeProtector off?

Article available in these languages: Spanish

Issue:

Why is the Protection Working LED of an APC SurgeArrest, or SurgeProtector off?

Product Line:

APC Surge Arrest

Environment:

N/A

Cause:

Reasons the green-colored Working Protection LED of the APC SurgeArrest may not

illuminate:

1. The unit is powered off (for 7 outlet SurgeArrest strips only).

2. The LED is defective.

3. The unit sustained a large power transient and basically died.

4. The unit was heavily overloaded and an internal fuse was tripped.


Resolution:

If one of the items numbered 2 through 4 is the reason, APC will replace the SurgeArrest under its lifetime warranty. First, check that the SurgeArrest unit's circuit breaker is not tripped. Then check that the SurgeArrest unit is plugged into a good, properly functioning power receptacle outlet.

Schneider Electric Global