Browse FAQs

What is the part number for the cooling fan for the ATV71HD30M3X?

Published date: 26 October 2018

Issue:   What is the part number for the cooling fan for the ATV71HD30M3X?
 
Product Line:   ATV71
 
Environment:  ATv71HD30M3X
 
Cause:   Replacement fan
 
Resolution:   
VZ3V1207 is the heat sink fan kit.  Each fan measures 3.62 by 3.62 inches.  A single fan is not available, order the complete kit.  The kit contains two fans and this drive uses one fan kit per drive. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.