Browse FAQs

How do I change the Profibus address on the ATV61 or ATV71 with an optional Profibus card?

Published date: 07 May 2019

Issue:
How do I change the Profibus address on the ATV61 or ATV71 with an optional Profibus card?  

Product Line:
Altivar 61, Altivar 71

Environment:
Profibus network

Cause:
Configuration

Resolution:

Profibus card part numbers are VW3A3307 or VW3A3307S371.

The profibus address is set through a series of 8 dip switchs on the card beside the 9 pin profibus connector.  The address is set in binary form.  A switch in the up position indicates 0 and in the down position indicates 1.  The least significant bit is the far right switch. Example, to set the address to 36 (binary 00100100).  Place the switches in order from left to right: UP, UP, DOWN, UP, UP, DOWN, UP, UP.



Refer to page 11 in either of the attached Profibus manuals for switch configurations. You can also download the manuals using these links:

ATV61/71 Profibus DP manual - VW3A3307
https://www.se.com/us/en/download/document/1755873/

ATV61/71 Profibus DPv1 manual - VW3A3307S371:
https://www.se.com/ww/en/download/document/AAV52935/

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.