{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How can the ATV61 drive be prevented from going into reverse when the HMI dial is turned to the negative range?

Issue:
Getting reverse rotation when HMI dial is turned to negative range.

Product Line:
Altivar 61

Environment:
All models

Cause:
N/A

Resolution:
In Menu 1.6 COMMAND, set RV Inhibition to Yes.  This also applies to the ATV71 drives.
Note that this does not prevent reverse operation when the request is sent by logic input.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Schneider Electric Global