Browse FAQs

Why does the ATS22 soft starter cost less than the ATS48, when the ATS22 has an internal shorting contactor?

Published date: 20 August 2018

Issue:
Why does the ATS22 soft starter cost less than the ATS48, when the ATS22 has an internal shorting contactor?

Product Line:
Altistart 22 and Altistart 48 Soft Starters

Environment:
All

Cause:
Curious about price difference between models of Soft Starters

Resolution:
The ATS48 is a more robust soft starter that can handle a wide range of applications.  A shorting contactor is recommended for all applications.

The ATS22 soft starter is not as robust, but does include an internal shorting contactor.  It is ideal for variable torque fan and pump applications.  It can also be used on constant torque applications with starting amps less than 3.5X ATS22 rating.  It is not recommend for heavy  loaded  or heavy duty constant torque applications. The ATS22 is generally priced lower than the ATS48.


CTA-ID : 2062515

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.