What can cause a ILF fault on the ATV71 drive with an VW3A3501 CIC card installed?
Published date:
01 November 2018
Issue:
What can cause a ILF fault on the ATV71 drive with an VW3A3501 CIC card installed?
Product line:
Altivar ATV71
Environment:
All models, all serial numbers
Cause:
If the CIC card is missing the external +24vdc pwr supply the drive will trigger an ILF fault after 1 sec of being powered up.
Resolution:
Per the CIC installation manual document, atv71_controller_inside_EN_V3 page 10, it is recommend to add an external power supply part number ABL7RE2402 to the controller inside cards +24vdc and com terminals to resolve issue.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.