{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can the Econoflex FLEX58 drive be replaced?
Issue:
The FLEX58 drive used in the Econoflex has failed and needs to be replaced.

Product line:
Econoflex FLEX58

Environment:
All models, all serial numbers

Cause:
Attempting to maintain the Econoflex and change just the FLEX58 converter.

Resolution:
The FLEX58 is still a repairable product.  Recommend removing the FLEX58 from the Econoflex enclosure and sending it to our repair facility.
Another option is to replace the entire Econoflex with a comparable ATV660 or S-Flex (ATV212).

Schneider Electric Global