Video: ATV312 - How to use logic inputs for up and down speeds.
Published date:
09 May 2019
Issue:
How can I program the drive to use logic inputs to speed up and down the motor?
Product line:
Altivar 312
Environment:
All models, all serial numbers
Resolution:
Program the following parameters
Under CTL menu:
LAC= L2 or L3 (hold for 3 seconds) Access Level
Under FUN menu, UPD-
rFC= Fr2 Ref. 2 switching
USP= LI3 (+) speed assign.
dSP= LI4 (-) speed assign.
Fr2= Updt Reference 2 Channel
When LI3 is enabled the motor will speed up.
When LI4 is enabled the motor will slow down.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.