{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Are the NetShelter CX and CX Mini delivered fully assembled?
Issue:
Need to know if the NetShelter CX and Mini arrive assembled.

Product Line:
NetShelter CX

Environment:
All versions and serial ranges.

Cause:
Customers may ask if assembly is required.

Resolution:
The NetShelter CX Mini arrives on its castors with the brush strip attached to the underside, on a pallet, and the keys inside.
The NetShelter CX arrives on a pallet with ramps supplied. The PDU power cord, leveling feet, keys and documentation are packed separately inside the cabinet.

Schneider Electric Global