Issue:
DC choke dimensional size used with an ATV61HC25N4 and ATV61HC40N4.
Product line:
Altivar ATV61
Environment:
Part number specific, all serial numbers
Cause:
None
Resolution:
The DC choke used with these models is designated DC-CHOKE 3.
There are 2 units per ATV61HC25N4.
There are 3 units per ATV61HC40N4.
See the attached file for dimensional information.
DC choke dimensional size used with an ATV61HC25N4 and ATV61HC40N4.
Product line:
Altivar ATV61
Environment:
Part number specific, all serial numbers
Cause:
None
Resolution:
The DC choke used with these models is designated DC-CHOKE 3.
There are 2 units per ATV61HC25N4.
There are 3 units per ATV61HC40N4.
See the attached file for dimensional information.