Browse FAQs

How can I monitor the logic inputs status in Ethernet TCP/IP for ATV61 and ATV71 ?

Published date: 13 July 2020

Issue:
Monitoring the logic input map to determine status of the logic inputs.

Product Line:
Altivar 61/71

Environment:
All Models and serial numbers.  Ethernet IP with Assemblies 100 and 101 with Profile as I/O

Cause:
None

Resolution:
To monitor the state of the logic inputs add logic address 5202 in the input scanner.  This is a read only and allows monitoring of the logic input map.  The map is as follows.
Bit 0 is LI1
Bit 1 is LI2
Bit 2 is LI3
Bit 3 is LI4
Bit 4 is LI5
Bit 5 is LI6

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.