{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can an ATV212 be used for single phase input applications?

Issue:
Is ATV212 capable of single phase input?

Product Line:
Altivar ATV212

Environment:
All serial numbers

Cause:
Some drives can be used with single phase supply voltage for three phase motors.

Resolution:
No, the Altivar 212 can only be used with three phase supply voltage to run three phase motors.

Schneider Electric Global