{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

PowerChute Network Shutdown v3.1 cannot connect to vCenter Server or ESXi hosts to perform VM and host tasks

Issue:
PowerChute Network Shutdown connects to vCenter Server/ ESXi Host Web Services using the URL "https://<IP Address>/sdk" using TCP port 443. If the TCP port is changed to a non-default port, PowerChute will not be able to connect.

Product Line:
PowerChute Network Shutdown v3.1

Environment:
VMware

Cause:
PowerChute only allows connection using port 443.

Resolution:
Upgrade to PCNS version 4.x
Or
Port 443 must be used.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
{"support":{"yesButton":"yes","noButton":"no","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Did this answer your question?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please check the box"}}}