{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How deep must the AR7580A Cable Manager be installed so the AR7581A Hinged Cover can open 90 degrees?
Issue:
Need to make sure the cover opens far enough to install and maintain cables.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
Customer needs to be able to fully open the hinged cable cover to add, move or change cables.

Resolution:
The AR7580A cable manager needs to be installed at least 10.5" deep in order for the AR7581A hinged cover to open a full 90 degrees.
Also see attached file for photo.

Schneider Electric Global

Attachment(s)
20140115 AR7580A Installation Depth.pdf [362.29 KB]