Browse FAQs

Why can't I add an input or output to my DFB I created in PL7pro ?

Published date: 31 October 2019

Issue: 
Unable to modify DFB in PL7 pro software


Product Line:
PL7Pro


Resolution:
To be able to edit your DFB's I/O you will have to remove any instance that is in use from your application code, then delete the instance from the list of "DFB Instances" under the "Variables" folder.
If this is not done it will not allow any edits to the DFB's I/O..


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.