Browse FAQs

What could cause the reference data from a Modsoft program not to be converted when using the Proworx 32 import function?

Published date: 03 June 2020

This will happen if the Modsoft program was never transferred from PLC to File in the Modsoft software. The reference data is not built into the Modsoft files until after a read from the PLC.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.