Browse FAQs

What is the cable needed to connect the M340 to the XBTGT 2xxx terminals?

Published date: 31 October 2019

Issue: 
cable needed to connect the M340 to the XBTGT 2xxx terminals


Product Line:
M340, XBTGT


Resolution:
The cable combination that is needed is the XBTZ938 + XBTZG909. It will connect the M340 to the following Magelis terminals:
XBTGT2110
XBTGT2120
XBTGT2130
XBTGT2220
XBTGT2330
XBTGT4230
XBTGT4330
XBTGT4340
XBTGT5230
XBTGT5330
XBTGT5340
XBTGT6330
XBTGT6340
XBTGT7340.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.