Browse FAQs

What are the differences between HMIGTW7353 and HMIGTW7354?

Published date: 01 November 2019

Issue: 
Differences between HMIGTW7353 and HMIGTW7354


Product Line:
Vijeo Designer, HMIGTW


Resolution:
Below are the differences between the GTW7353 and GTW7354 Magelis targets:
HMIGTW7354 - Open Panel 15" GTW DC
- Atom 1.10 GHz processor <---------
- 2GB Compact Flash card <---------
- Windows® Embedded Standard 2009 <---------

HMI GTW7353 - 15" LCD TFT
- Intel Celeron M 1GHz processor<----------
- 4GB Compact Flash card <----------
- Windows® XP Embedded <---------



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.