Browse FAQs

How to add an EDS file to the DTM library in EcoStruxure Control Expert?

Published date: 24 October 2019

Issue:
How to add an EDS file to the DTM library in EcoStruxure Control Expert?

Product Line:
M340
M580

Environment:
Ecostruxure Control Expert
Unity Pro

Resolution:
First you need to select with your mouse the NOC Scanner module in the DTM Browser and right click.
The right click menu will display and then you would select 'Device Menu' and then 'Add EDS to library'
See screen shot example below.


The EDS Addition window will open and you select Next. see below.



Next select the appropriate radio button and then click Browse to navigate to the location of the EDS file.



After selecting your File(s) a window will open that displays the status of the EDS file.
If the file has no errors then you can select Next. See below.


Click Next and then Finish.



Remember to Updated and Reload your DTM Catalog to have access to the newly added EDS file.


Legacy KB System (APS) Data: RESL209894 V1.0, Originally authored by BrWa on 12/06/2012, Last Edited by BrWa on 12/06/2012
Related ranges: Unity Pro - SoCollaborative software, ConneXium - Ethernet

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.