Browse FAQs

How many concurrent TCP connections can be supported by the Advantys OTB module?

Published date: 23 October 2019

Issue:
How many concurrent TCP/IP connections can the Advantys OTB have?

Product line:
Advantys OTB

Environment:
Advantys COnfiguration software

Cause:
To determine how many concurrent connections that the OTB1EODM9LP can have. 

Resolution:
The Advantys OTB Ethernet NIM will allow 3 concurrent ModbusTCP Port 502 connections.

Note: The OTB and the TM2 I/O modules will be obsolete in Oct. 2018 and the recommended replacement would be the TM3BCEIP  Distributed Optimized TM3 Bus coupler. 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.