Browse FAQs

What are the Twido TWDXPCRTC Real Time Clock option adapter specifications?

Published date: 11 November 2019

Issue:
Twido RTC specifications.

Product line:
Twido

Environment:
TwidoSoft or TwidoSuite

Cause:
Information on the different specifications on back up and charging time.

Resolution:
The below chart is for the Twido TWDXCPRTC Real Time Clock specifications.

ACCURACY
30 s/month (typical) at 25 DEG C (77 deg.F)
Backup duration Approximately 30 days (typical) at 25 Deg. C (77 deg.F) after backup battery fully charged.
Battery Lithium secondary battery
Charging time Approximately 10 hours for charging from 0% to 90% of full charge
Replaceable Can Not replace battery

Note: The Twido was obsolete 12/31/2016 and was replaced with the M221 and the M221 has a replaceable battery.
 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.