Goals and Symptoms
There is somthing confusing about the current derating with the altitude > 1000m. The data in catalogue is 2.2% per additional 100m while in manual is 0.5%.
Which one is right?
Facts and Changes
ATS48
Altitude
Causes and Fixes
These both values are bad. The real derating is 2% per additional 100 meter.
Legacy KB System (APS) Data: RESL156259 V3.0, Originally authored by on , Last Edited by on
Related ranges: Altistart 48
Released for:Schneider Electric Global