Can the 170ENT11001 or 170ENT11002 be used as a replacement for the 170ENT11000?
Published date:
31 July 2019
Issue:
Can the 170ENT11001 or 170ENT11002 be used as a replacement for the 170ENT11000?
Product Line:
Momentum
Environment:
Windows Command Line interface
Resolution:
The 170ENT11002 can be used as a direct replacement for the 170ENT11000 since both products do not have web page access.
The 170ENT11001 can be used as a replacement for the 170ENT11000 however, the set up and configuration of the IP address and communication is quite different. The 170ENT11001 is a 10/100 base-T Ethernet with auto sensing and detection. This Module also supports FDR (Faulty Device Replacement). You must download the user manual for the 170ENT11001 in order to learn how to work with this new module. Many of the configuration steps have changed.