Browse FAQs

Is it possible to flash the executive firmware of the TSX Momentum 171CCC96020 and 171CCC98020 M1E CPU's to accept IEC programming?

Published date: 31 October 2018

No, the TSX Momentum 171CCC96020 and 171CCC98020 M1E CPU's are only compatible with 984 Ladder Logic. However, the 171CCC96030 and the 171CCC98030 are 984 Ladder Logic and IEC compatible depending on the firmware that is downloaded into them.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.