Browse FAQs

What is the purpose of the 'Add hyperlink' function in Unity Pro?

Published date: 30 August 2018

Hyperlink allows the user to create a link between the project and external documents or applications. Right click on a project section and choose 'hyperlink' to specify a document or application location. A link can also be added to the comment field in animation tables, data editor variables, operator screens and documentation.


Legacy KB System (APS) Data: RESL170338 V1.0, Originally authored by on , Last Edited by on
Related ranges: Unity Pro

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.