Browse FAQs

What are the Telefast fuse part numbers?

Published date: 10 July 2020

The following fuse part numbers are used in the Telefast 2 PreWired System Connection Interfaces:

Fuse Rating
Part Number
0.125 A
ABE7FU012
0.5 A
ABE7FU050
1 A
ABE7FU100
2 A
ABE7FU200
4 A
ABE7FU400
6.3 A
ABE7FU630

These fuses are fast blow, 5 x 20mm, 250V and have a quantity of 10 per package.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.